ZigBee MC13193 general questions

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

ZigBee MC13193 general questions

1,970件の閲覧回数
sayantist
Contributor I
Hi
I am new to Zigbee and i am plan to use the MC13193. My question is, does it need to have a line of sight between the coordinator, and end devices? Does the end devices need to have a line of sight with the router/ coordinator?
Also, does using the antenna strip, particularly the F-antenna (embedded in the PCB) give a reliable signal or i will need to have an externa antenna, especially the place has many obstacles? What is the range of the F-antenna (embedded in the PCB). Does it have to be line of sight?
ANy suggestion would be a great help.
Thanks!:smileyhappy:

Message Edited by Alban on 2006-11-13 12:24 PM

ラベル(1)
0 件の賞賛
返信
1 返信

883件の閲覧回数
peg
Senior Contributor IV
0 件の賞賛
返信