ZigBee Binding Confusion

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

ZigBee Binding Confusion

2,134 Views
zoz
Contributor I

I have a question regarding ZigBee binding.

 

I have a switch and I would like to bind that switch to 3 lamps (the example in the ZigBee documentation). After binding these lamps to the switch I would like to turn on/off the lapms individually. The idea is to have a mobile swtich which could turn off and on all lamps in the house. Is it possible to do this?

Labels (1)
0 Kudos
Reply
1 Reply

1,418 Views
Mads
Contributor V

Hi,

 

When using binding you need to consider the "endpoint" like a switch on the wall.

Controlling 3 lamps individually can not be done using just 1 switch :smileyhappy:

 

If you want to use binding, you will need to have 3 switch applications in your device, else you can not bind each "switch"/endpoint to an individual lamp.

 

Another option is to send the on/off command directly to each indivual lamp. this only requires one endpoint but requires you know the destination endpoint and address.

 

I can recommend that you acquire Drew Gislason's book : "ZigBee Wireless networking" as a add on to reading the ZigBee specificaton.

 

br,

Mads

0 Kudos
Reply