ZSTAR3 (HCS08): Is it possible to change a sensor's index?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

ZSTAR3 (HCS08): Is it possible to change a sensor's index?

2,220件の閲覧回数
monpat
Contributor I

Hello everybody

 

I work with several zstar3 sensors and I would like to change their IDs (index). Is there a command for this?

 

Thanks!

monpat

ラベル(1)
0 件の賞賛
返信
2 返答(返信)

1,450件の閲覧回数
Gargy
NXP Employee
NXP Employee

Hi,

 yoe there is command to change sensors ID. There is two possibilities how to change this ID:

1. If you a re using the zstarlib.dll library, the situation is easiest - It must be called (when sesor is connected) theSensor.IndexSet(newIndex) method.

 

2. If you are communicated directly over serial/USB protocol - It must be sends command 'F'and new index to active sensor.

 

Have a nice day

0 件の賞賛
返信

1,450件の閲覧回数
drfordo
Contributor I

But how could i change it .My sensor dosn't active .although my usb receiver connect to zstar3 and active .I mean the programm found  usb receiver but sensor doesn't work. I guss this proplem happend becaus i try to change simple rate data(form 30HZ to 60HZ) before i change index .

 

please help me to make my sensor work again

this is my email: [email protected]

0 件の賞賛
返信