Wire GR8 For Real World Use?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Wire GR8 For Real World Use?

3,025 Views
AveryZ
Contributor I
Hi,

I have a GR8 that I built a programmer for, loaded with code, and now I am ready to move it into its actual real home. I am having trouble figuring out how to wire it so that when it recieves voltage/turns on, it just jumps right into the program code thats on it.

Forgetting about where I/O is wired, I connected Vdd and Vss, Vdda and Vssa, and Vdda/ref and Vssa/ref to ground and voltage respectively. I have also connected OSC1 to my crystal which is 9.8304. Is there anythign else that should be wired?

Also I am communicating with the PC over SCI, and I have the two wires plugged directly into their respective ports on the chip, should they be going through a MAX232?

Thanks Guys!
-Avery
Labels (1)
0 Kudos
Reply
2 Replies

1,790 Views
AveryZ
Contributor I
Mac,

Thanks so much for your speedy response! I will implement these changes immedietly! I don't think the chip is damaged from the SCI already, b/c I can put it back into monitor mode and it works fine, but we'll see!

Thank You!
-Avery
0 Kudos
Reply

1,790 Views
bigmac
Specialist III
Hello Avery,


Avery Z wrote:

...  I connected Vdd and Vss, Vdda and Vssa, and Vdda/ref and Vssa/ref to ground and voltage respectively. I have also connected OSC1 to my crystal which is 9.8304. Is there anythign else that should be wired?

Did you provide separate de-coupling capacitors at each of the supply connection points, as specified in the data sheet?  Did you connect the crystal as a Pierce oscillator configuration, as shown in Fig. 28 of the data sheet?  This involves connections to both OSC1 and OSC2.  For a 9.8304 MHz crystal, the resistor Rs can usually be omitted, and make C2 a fixed capacitor of the same value as C1.  What component values do you currently use.


Avery Z wrote:
 
Also I am communicating with the PC over SCI, and I have the two wires plugged directly into their respective ports on the chip, should they be going through a MAX232?

Very definitely.  You may have already damaged the chip!
 
Regards,
Mac
 
0 Kudos
Reply