Unknown Base Plugin Nub Error

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Unknown Base Plugin Nub Error

2,053 Views
tcherno
Contributor II

hello,

I have a project in Code Warrior 10.6.4 IDE developed for MC9S08QE128 MCU.

I am using PE micro Multilink FX as a debugger and programmer.

 

until a week ago I was able to debug and burn the code. to the flash of the MCU with no problem.

now when i try to debug or burn the code i get the error "Unknown Base Plugin Nub error".

 

with the PROGHCS08 - Flash Programmer Software from PE micro i have no problem burning the code on the board with the same debugger.

 
when checking the signal of the BDM, i can see that the PC tried to initiate connection with the MCU.

 

have anyone faced this problem and can help me?

 

thank you,

omer

0 Kudos
Reply
0 Replies