Time on simulation

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Time on simulation

2,160 Views
mohammed
Contributor III
Dear All;
am running <Full Chip Simulation>;  need to monitor time;
there is a timer interrupt, that occur every specific period, need to see in simulation window; when timer overflow?, when interrupt happened?;
 
the question is, is there is a window that shows the real time,
 
BTW; PLL is set to 16MHz, 4MHz Fbus;    i change the frequency in the simulation and replaced the 9.8MHz with 16MHz;
 
Please Advice
 
Labels (1)
0 Kudos
Reply
1 Reply

1,404 Views
mohammed
Contributor III
GOT IT, thanks anyway,
0 Kudos
Reply