The Classification and Application of Microcontrollers

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

The Classification and Application of Microcontrollers

1,997 Views
xiaoye
Contributor I

Microcontrollers are classified into two types based on their memory type: those with no on-chip ROM  and those with on-chip ROM,  The chip without on-chip ROM  must be used externally with EPROM (typically 8031); the chip with on-chip ROM  is classified as on-chip EPROM (typically 87C51), MASK on-chip mask ROM  (typically 8051), on-chip Flash (typically 89C51), and other types.

MCUs are classified into two types based on their intended use: general-purpose and special-purpose. It is classified into4, 8, 16, and 32-bit MCUs based on the width of the data bus and the number of data bytes that can be processed at the same time.

0 Kudos
Reply
0 Replies