TPS with MC33794 E-field sensor

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

TPS with MC33794 E-field sensor

3,294 Views
sec1980
Contributor I
hi to all.
i'm working with the touch panel system which contain the MC33794 E-field sensor.
i've tried to program the MC68HC908QB8 integrated in the platform an then i lost the original firmware contained.
Would it be possible to have this firmware, to eventually modify it and use for my exam?
please answer as soon as possible.

regards
Labels (1)
0 Kudos
Reply
2 Replies

1,482 Views
alex_spotw
Contributor III
HI:

It would be helpful to know which touch panel system you're talking about...

You might want to contact directly the manufacturer, but I doubt they will give you the source code (or any code for that matter).

Regards,

Alex
0 Kudos
Reply

1,482 Views
sec1980
Contributor I
i'm working with the demo board described in this reference manual:

http://www.freescale.com/files/analog/doc/ref_manual/MC33794RM.pdf

you can find it under the menu product -> sensor -> e-field sensor

the reference manual contain information about some functions contained in the original firmware of the board, so i thinked that this firmware was free to use...

please tell me if there is someone to contact to obtain this firmware; it's very important because this is for my last exam at university...

regards
0 Kudos
Reply