TPS with MC33794 E-field sensor

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

TPS with MC33794 E-field sensor

3,289件の閲覧回数
sec1980
Contributor I
hi to all.
i'm working with the touch panel system which contain the MC33794 E-field sensor.
i've tried to program the MC68HC908QB8 integrated in the platform an then i lost the original firmware contained.
Would it be possible to have this firmware, to eventually modify it and use for my exam?
please answer as soon as possible.

regards
ラベル(1)
0 件の賞賛
返信
2 返答(返信)

1,477件の閲覧回数
alex_spotw
Contributor III
HI:

It would be helpful to know which touch panel system you're talking about...

You might want to contact directly the manufacturer, but I doubt they will give you the source code (or any code for that matter).

Regards,

Alex
0 件の賞賛
返信

1,477件の閲覧回数
sec1980
Contributor I
i'm working with the demo board described in this reference manual:

http://www.freescale.com/files/analog/doc/ref_manual/MC33794RM.pdf

you can find it under the menu product -> sensor -> e-field sensor

the reference manual contain information about some functions contained in the original firmware of the board, so i thinked that this firmware was free to use...

please tell me if there is someone to contact to obtain this firmware; it's very important because this is for my last exam at university...

regards
0 件の賞賛
返信