Serial protocol

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Serial protocol

1,980 Views
karthick1987
Contributor II

HI guys,

 

I am using a GT16A micro and I was wondering if the serial communication protocol can be changed. Normally we have

 

Start bit + 8/9 bits + stop bit

 

Is it possible to have

 

8/9 bits + stop bit ?

 

If yes how can I do that ? 

Labels (1)
0 Kudos
Reply
2 Replies

1,535 Views
rocco
Senior Contributor II

No, it is not possible to eliminate the start-bit.

 

Without a start-bit, how would you know when a transfer has started?

0 Kudos
Reply

1,535 Views
karthick1987
Contributor II

I thought of that too but I am using an Xbee which runs a different protocol. Apparently it only has a the transfer bits + parity + Stop bit. this is a bit bizarre. but I will look into it further.

 

cheers

k

0 Kudos
Reply