Serial based firmware update? - MC9SO8GT16A

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Serial based firmware update? - MC9SO8GT16A

3,330件の閲覧回数
Kerms
Contributor I
Hello,
 
I am trying to utilize an MC9SO8GT16A in a product, and I wanted to know if it is possible to update the firmware via its serial port.
 
I would like to be able to provide a way to reprogram the device from the computer, but I am not sure if this chip can do so.
 
Any suggestions would be apprecited.
 
 
 
 
 
Added p/n to subject.


Message Edited by NLFSJ on 2007-12-17 07:54 AM
ラベル(1)
0 件の賞賛
返信
4 返答(返信)

2,235件の閲覧回数
peg
Senior Contributor IV
Hi Kerms,

The short answer is, Yes!

For some longer answers take a look at AN2140 and AN2295.
Also this subject has been discussed here quite a bit, but not very recently.

0 件の賞賛
返信

2,235件の閲覧回数
Kerms
Contributor I

Hi Peg, Thanks for the info. I am doing my best to read though and try to understand the material there. 

First question, is the MC9S08GB60 code compatible with the MC9S08GT16A?

0 件の賞賛
返信

2,235件の閲覧回数
Kerms
Contributor I
K finished (well mostly) skimming through AN2295 and wow that is exactly what I was looking for!
 
But... I am lost. Not quite sure how the src names are labeled.
 
I've used the MC9S08QG8 before, and clearly there is a S08QG folder, but what about the GT16A?
 
Is that the S08GBGT folder?
 
Any help would help a lot!
 
Thank you!
0 件の賞賛
返信

2,235件の閲覧回数
peg
Senior Contributor IV
Hi Kerms,

The GT is just a "cut down" version of a GB. The 16 just has less memory than the 60.
The GTxxA is an upgraded version of the GTxx.
Just be wary of what the GT16 lacks compared to the GB60 and use EB671 to be aware of the differences between non-A and A.
Most of the time you don't have to be concerned at all!
I am not sure what you are talking about with the "folders". Codewarrior?

0 件の賞賛
返信