SMAC problem with NCB board - have yu experienced the same?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

SMAC problem with NCB board - have yu experienced the same?

3,289 Views
zoz
Contributor I
I am trying to use SMAC demo applications on NCB boards: Repeater, Lighting demo(controller and device). Lighting demo - controller works good (transmitting messages ok).
But neither the lighting device nor the repeater application receives properly! The repeater sometimes receives a packet but very rarely and the received data is not correct.
I have tried BeeStack CodeBase and MAC Codebase applications as well on the same boards and they all worked perfectly - so the boards are good.
I have tried SMAC demo appliactions on SARD boards as well and they all performed good!
 
So I presume there is something wrong in the SMAC codebase when it is applied to NCB boards. The problem is with receiving, the transmitting works perfectly.
 
Have you experienced the same problem??
Labels (1)
0 Kudos
Reply
3 Replies

2,017 Views
zoz
Contributor I
The problem only occurs in promiscous mode... but why?
0 Kudos
Reply

2,017 Views
Alex_RUS
Contributor I
I am sorry.
Could you say in couple of words what is "promiscous" mode. What means "promiscous"?? Thank you.
0 Kudos
Reply

2,017 Views
peg
Senior Contributor IV
Hi,
 
Promiscuous:
1. having an indiscriminate number of casual sexual relationships.
2. Lacking order.
 
I will leave it to you to apply it to SMAC.
It was spelt wrongly before.
 
0 Kudos
Reply