SMAC and BeeStack together

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

SMAC and BeeStack together

2,548件の閲覧回数
Rafael_21
Contributor I
Is it  possible to connect a SMAC device to a Beestack device?

Is it transparent to me? Or I need to program something?

thank you!
ラベル(1)
0 件の賞賛
返信
2 返答(返信)

1,504件の閲覧回数
NLFSJ
Contributor III
Hi
 
SMAC devices cannot directly connect to a ZigBee Network as they have different networking layers.  The only way to do this is via a gateway device that will do translation from one network to the other. 
 
    
 
 
 
 
Regards,
Nina
0 件の賞賛
返信

1,504件の閲覧回数
Mads
Contributor V
Hi,
SMAC is NOT compliant with 802.15.4 which ZigBee is build on top.
the SMAC is not compliant with the very strict timing and SMAC does not provide the acknowlegdement scheme as 802.15.4
 
Br,
Mads
0 件の賞賛
返信