S908EL/SL availablity in extended temperature range

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

S908EL/SL availablity in extended temperature range

1,738件の閲覧回数
andy_sinclair
Contributor I
I am sourcing a new low end micro for possible forthcoming projects.

The EL/SL range are tempting as they include EEPROM and are attractively priced.
We do require extended temperature range however (-40 to 125) which does not seem to be easy to obtain.

Are extended temperature versions of these devices going to be widely available later in the year?
If not, what sort of price premium over commercial parts and MOQ is involved if ordering an automotively qualified device.
ラベル(1)
0 件の賞賛
返信
1 返信

1,105件の閲覧回数
NLFSJ
Contributor III
Hi,
 
I believe this was also submited via a service request. 
 
The reply is -
 
Yes, there will be a M temp device (-40 to 125) and  V temp (-40 to 105).  The adders are 10% and 5% above the C temp price (-40 to 85).
The M and the V are in the part numbering scheme, i.e. M and then the package designation, V and then the package designation.
 
Regards,
Nina
0 件の賞賛
返信