S08CRCV1  Modbus RTU CRC

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

S08CRCV1  Modbus RTU CRC

1,949 Views
OneBitBrain
Contributor II

Is the S08CRCV1 capable to calculate the Modbus RTU CRC?

 

I have tried all combination for the seed, with no sucess.

 

Thanks.

Labels (1)
0 Kudos
Reply
2 Replies

1,559 Views
kef
Specialist I

S08CRCV1 supports only CRC16-CCITT, which has different polynomial that one used in Modbus.

PCRCV1 module, available on S08GW, has programmable polynomial and thus can work CRC16, CRC16-CCITT and others.

0 Kudos
Reply

1,559 Views
OneBitBrain
Contributor II

Thanks.

I cannot change the device at this time, but in the future your sugestion can be useful. Better if there was one CRC hardware for each SCI port, but nothing that cannot be solved with software interlock.

0 Kudos
Reply