Relative values of A2D Input Leakage Currents

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Relative values of A2D Input Leakage Currents

863件の閲覧回数
stephenwhite
Contributor I

The S9S08RNA16W2MLCR A2D data sheet specifies the range of input pin leakage currents as  -1uA to +1uA.  I have high impedance series input resistors (500Kohm to 1MHom) to a pair of analog signals the connect to two microcontroller A2D input pins.   Can I assume that the leakage currents of the two A2D input pins will match if the input voltage are the same?  That is, if one pin leaks 1uA , will the other pin leak 1uA as well if both input voltage are the same?

ラベル(1)
タグ(1)
0 件の賞賛
返信
0 返答(返信)