RF Signal transmission with TWR 12311

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

RF Signal transmission with TWR 12311

1,215件の閲覧回数
MW57
Contributor I

Hi !

I intend to transmit signals (generated by sensors) between two TWR 12311 bords with acquisition of the signals via the onboard ADC of the emitter board and reception of the signals via RF on the reception board. The acquired signals are then transmitted to a computer per Ethernet for processing and displaying through a C++/QT HMI. 

I find this job very difficult. Can some one help ? Is there some sample code anywhere on the internet or in the Bee Kit codebase that can help namely for the manipulating of the ADC ? The microcontroller is the HCS08.

Thanks in advance for your answer.

タグ(1)
0 件の賞賛
返信
0 返答(返信)