QG8 flash write on LVD interrupt

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

QG8 flash write on LVD interrupt

2,193件の閲覧回数
glennk
Contributor I
I would like to use the LVD interrupt to save one byte of data to flash in the QG8 part when power is going down.  The flash will already be erased, so I'll only need to program the one byte as power goes down. I'm using CodeWarrior with Processor Expert.   I have two questions:
 
1. Can I write to flash from within the LVD interrupt using SetByteFlash?
 
2. What is the safest thing to do after the flash is programmed?  I don't want the code to run amuck as power goes down.  Is there any software way of forcing the chip into reset?
 
Thanks
ラベル(1)
0 件の賞賛
返信
2 返答(返信)

1,396件の閲覧回数
bigmac
Specialist III
Hello,
 
It should be feasible to program the byte value to flash within the ISR code.  Of course, the code that controls the programming process will actually be running from RAM (probably the stack).
 
After programming is complete, I guess there are a couple of possibilities -
  1. Enter a wait loop within the ISR, and rely on the COP timer to initiate a reset.
  2. Execute an illegal opcode within the ISR to immediately initiate a reset.
 
One thing you may have to guard against is the occurrence of multiple LVD interrupts should reset initialisation occur more than once for the same power event.  Ideally, the LVD should interrupt the first time, and hold a reset condition the second time.  The problem will be detecting which is first and second time.
 
Regards,
Mac
 
 
0 件の賞賛
返信

1,396件の閲覧回数
bigmac
Specialist III
Hello,
 
A further thought on the multiple interrupt/reset issue.
 
Assuming you were to cause an immediate reset using the illegal opcode method (after programming the flash byte), since the SPMSC1_LVDRE bit is set out of reset, I assume a reset condition would be held during the remainder of the power-down process.  If this be true, then multiple resets or interrups could never occur during a power "ramp down".
 
Regards,
Mac
 


Message Edited by bigmac on 2007-12-20 12:50 PM
0 件の賞賛
返信