Problems with demoboard Demo9s08qg8

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Problems with demoboard Demo9s08qg8

6,600件の閲覧回数
zetorista
Contributor I
Hi guys,
I tried a demo board DEMO9S08QG8 and propably I burned one part (chip) which is called U305. I cannot find board schematics which including this part. Do you have any suggesting about that?
ラベル(1)
0 件の賞賛
返信
11 返答(返信)

3,904件の閲覧回数
thisobj
Contributor III
Hello,

U305 IC-Switch-Smt (DCT8) SN74LVC2G66DCT, Analog Sw,Bilateral,Dual Digi-Key 296-13271-1-ND

The BOM for this board is included in "DOC-0363-010 REV E" from Axiom, who made the boards. It is called "DEMO9S08QG8_UG.pdf" and is part of the pdf document set on the Axiom Support CD. The problem is that the latest version, Rev F, (on their web site) calls out one revision: "Remove BOM". Apparently, REV E had a very short life, as it is dated Feb 16, 2006. REV F is dated Mar 2, 2006.

Hopefully, there is no violation in posting the part info. I would be happy to upload the REV E doc, but only if Alban sees no problem in doing so.

Frank

Message Edited by thisobj on 2007-02-2808:38 AM

0 件の賞賛
返信

3,904件の閲覧回数
Alban
Senior Contributor II
Hello Frank,
 
Good search. If it is on Axiom website, you can certainly post it here.
In the schematics, the zone is hidden under "P&E BDM" - http://www.axman.com/?q=node/89.
 
As the info is distributed by Axiom, I don't see any violation.
Please feel welcomed to.
 
(I just didn't want to be beaten up by any of the two Companies)
 
Cheers,
Alban.
0 件の賞賛
返信

3,904件の閲覧回数
zetorista
Contributor I
HI ,
thanks guys, it helps me a lot.
0 件の賞賛
返信

3,904件の閲覧回数
thisobj
Contributor III
Hi Alban,

The problem is that on Axiom's web site, the Rev E doc, which included the BOM, has been replaced with the Rev F doc, which no longer includes the BOM. With all of that said, I have attached the Rev E doc here, with the full understanding that you may find it necessary to remove it if required.

Frank
0 件の賞賛
返信

3,904件の閲覧回数
Alban
Senior Contributor II
Hello,
 
You can use the search by part number. It gives you the product page which shows the following:
 
DEMO9S08QG8 Schematics  FREESCALE   zip   111KB    RevC  
 
It looks like what you want.
Cheers,
Alban./DIV>

Message Edited by Alban on 2007-02-26 05:59 PM

0 件の賞賛
返信

3,904件の閲覧回数
zetorista
Contributor I
Thanks for answer,
I have check that pdf but that one is not including USB-BDM part, so is not including U305
0 件の賞賛
返信

3,904件の閲覧回数
Alban
Senior Contributor II
Oups,
 
I didn't know you wanted this portion.
The USB BDM portion is protected Intellectual Property. In other words, it is confidential information...
 
Sorry,
Alban.
0 件の賞賛
返信

3,904件の閲覧回数
peg
Senior Contributor IV
Hi,
If this is the large IC in the BDM section then it is just a microcontroller which you can buy. However the firmware inside it is the problem. It is owned by P&E Microcomputer. You probably need to buy another one or buy a USB BDM module seperately.
 
0 件の賞賛
返信

3,904件の閲覧回数
bigmac
Specialist III
Peg, actually on my board U305 is small 8-pin package with the marking C6619Z.
 
It seems somewhat over-sensitive to me, for Freescale not to publish at least a BOM, so as to potentially allow for repair by the experienced user.  Especially since Freescale does not make spare parts available.  I would guess that most of the IP content is associated with the firmware within the MCU, rather than the identification of the components that are used on the board.
 
Regards,
Mac
 
0 件の賞賛
返信

3,904件の閲覧回数
peg
Senior Contributor IV
Hi Mac,
 
I popped open my USB BDM and it has two 8 pin devices:
 
a larger one:
MSC
34164
413A
 
and a smaller one:
C25
4AZ
 
perhaps this part is some of the extra circuitry to switch the Vcc to the QG to handle the lack of RST problem??? This may also be how/why it failed.
 
 
0 件の賞賛
返信

3,904件の閲覧回数
bigmac
Specialist III
Peg,
 
The larger device could be a MC34164, a low voltage reset device.  This is U301 on the demo board.  The other smaller device is U305 is the mystery device.
 
Regards,
Mac
 
 
 
0 件の賞賛
返信