Problem with SMAC 4.1

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Problem with SMAC 4.1

2,788件の閲覧回数
martyseb63
Contributor I
Hello I currently work on a MC9S08GT60 and with SMAC 4.1 to communicate with zigbee. To develop, I use codewarrior Special Edition. I have a problem when I want to send a packet. In MCPSDataRequest(), gu8RTxMode is set to TX_MODE. After there is a loop : while (gu8RTxMode != IDLE_MODE) In my program, the loop don't stop. I want to know how gu8RTxMode can be set to IDLE_MODE alone. The problem may comes from the librairie : I'm using SMAC_13192evb_4_1a.lib which correspond to my zigbee's module (mc13192). Can you help me if you have an idea. Thank
ラベル(1)
0 件の賞賛
返信
1 返信

1,308件の閲覧回数
alex_spotw
Contributor III
Hi:

Is your external interrupt set up correctly, both in HW and SW? The Mc13192 uses the external interrupt pin to indicate the GT60 to change modes. If the interrupt is not recognized, or clear, or never arrives, then the SMAC won't change mode.

There are also some issues with reentrancy of the interrupt code in the SMAC, and you might need to check the actual SMAC code and see if your code is not breaking something in the SMAC (variables, etc)

Regards,

Alex
0 件の賞賛
返信