Power Cycle Dialog

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Power Cycle Dialog

Jump to solution
3,214 Views
benthie
Contributor II

Hello everybody,

 

I´m working with a MC9S08QB4 at the moment and my problem is, like the topic already said, the "Power Cycle Dialog". CodeWarrior (10.2) is telling me that the MCU is not responding. I´ve done some research about that problem and usually the first idea is to check the BDM-6Pin-Tool-Connector. I did that and have the following question:

 

Pin1 is connected to BKGD (PTA4) and VSS at the same time?

 

Because if I am not totally wrong, that is what the ReferenceManual (Rev.1, page 25) tells me.

 

Thanks and regards,

Ben

Labels (1)
1 Solution
2,840 Views
bigmac
Specialist III

Hello Ben,

The diagram that you refer to is faulty.  Pin 1 of the header is meant to connect to the BKGD/MS pin alone.  Pin 2 connects to ground.

Regards,

Mac

View solution in original post

0 Kudos
Reply
4 Replies
2,840 Views
Monica
Senior Contributor III

Hello Ben,

Has this fixed your issue? Don't forget to keep us posted :smileywink:

Best regards,

Monica.

0 Kudos
Reply
2,840 Views
benthie
Contributor II

That has fixed my problem, yes. Sorry for not evaluating the answer. I´m sort of a newbie here :smileywink:

Best regards,

Ben

2,840 Views
Monica
Senior Contributor III

No problem, we're happy to have you at Community! :smileygrin:

Great week!

Monica

0 Kudos
Reply
2,840 Views
bigmac
Specialist III

Hello Ben,

The diagram that you refer to is faulty.  Pin 1 of the header is meant to connect to the BKGD/MS pin alone.  Pin 2 connects to ground.

Regards,

Mac

0 Kudos
Reply