PWM Sine Wave Generation

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

PWM Sine Wave Generation

Jump to solution
7,026 Views
admin
Specialist II
Hello,

In the process of generating a sine wave to drive a 3-phase motor (via a 6-MOSFET or IGBT bridge), and using the V/Hz ramp technique, we can see that the V/Hz ramp process (reference. AN1857, AN1664, etc.) has two output variables:

Amplitude and Table_inc

These two variables are the input for the next process, the PWM Generation Process (Pwmcalc.c) , which, for phase A (for example), uses a sine wave table for one quadrant (with 3rd harmonic) (variable wavequad), retrieves the Table_value, then SCALES BY AMPLITUDE, and finally, calculates PVAL1.

A piece of the code follows:


Table_value = (wavequad[Quad_ptr>>8]); Pwmmod_wave = (Table_value * Amplitude); /* scale by Amplitude */
PVAL1 = (Pwmmod_wave>>8) + (PWM_MODULUS/2);


So my question is if we actually have the wavequad wave table for one quadrant, why do we have to scale Table_value by amplitude ? Isn't the data in the wave table sufficient for that ?

Second question follows: where can I find generous litterature about how is Amplitude related to PVALx's value, since PVALx is a register for the PWM module ?!! Can anyone explain that clearly please ?


Best Regards,
Roger Tannous.
Labels (1)
0 Kudos
Reply
1 Solution
2,516 Views
rocco
Senior Contributor II
Hi, Roger:

I think the mathematically correct way to look at the output is as a vector. A vector has an amplitude and an angle.

But the practical way of thinking about it is to compare your brushless-motor with a brushed-motor. A brushed-motor does it's own commutation, and all you need to do is provide a voltage or current (torque) command to control it. The amplitude, in your application is analogous to the voltage or current command, and the angle is the only the commutation.

View solution in original post

0 Kudos
Reply
1 Reply
2,517 Views
rocco
Senior Contributor II
Hi, Roger:

I think the mathematically correct way to look at the output is as a vector. A vector has an amplitude and an angle.

But the practical way of thinking about it is to compare your brushless-motor with a brushed-motor. A brushed-motor does it's own commutation, and all you need to do is provide a voltage or current (torque) command to control it. The amplitude, in your application is analogous to the voltage or current command, and the angle is the only the commutation.
0 Kudos
Reply