Not able to boot linux-2.6.25.3 ltib kernel on TX28 karo module

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Not able to boot linux-2.6.25.3 ltib kernel on TX28 karo module

1,384件の閲覧回数
venkatesh_kumar
Contributor I

Hi everybody,

 

I am using linux-2.6.35.3 ltib kernel for booting tx28 karo module. But we have done the pin muxing changes. Then also the kernel is not booting . Please refer the below log message.

 

Booting kernel from Legacy Image at 42000000 ...
   Image Name:   Linux-2.6.35.3-571-gcca29a0
   Image Type:   ARM Linux Kernel Image (uncompressed)
   Data Size:    2368916 Bytes =  2.3 MB
   Load Address: 40008000
   Entry Point:  40008000
   Verifying Checksum ... OK
   Loading Kernel Image ... OK
OK

Starting kernel ...

Uncompressing Linux... done, booting the kernel.

 

It stops at this point. Can anybody tell me should i make any another changes to overcome the above problem.

 

Rgds,

G.Venkatesh Kumar

ラベル(1)
0 件の賞賛
返信
1 返信

1,061件の閲覧回数
peg
Senior Contributor IV

Hello,

 

Your in big trouble if you think you are dealing with a 8-Bit microcontroller here!

Try here.

0 件の賞賛
返信