MMA7660FC: driver from Freescale?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

MMA7660FC: driver from Freescale?

1,815件の閲覧回数
Bobli
Contributor I

Hello,

 

I have a MMA7660FC installed on my board. I would like to know if there is any driver software available from Freescale showing how initialization can be done?

 

In http://www.freescale.com/webapp/sps/site/prod_summary.jsp?code=MMA7660FC&fpsp=1&tab=Design_Tools_Tab I found only a header file containing register definitions; Is there any application file showing how to use the register definitions to configure the device?

 

Bob

ラベル(1)
0 件の賞賛
返信
2 返答(返信)

1,588件の閲覧回数
bigmac
Specialist III

Hello Bob,

 

There appears to be a series of Application Notes that provide information, including setup, for a number of different applications for the accelerometer.

AN3837, AN3838, AN3840 and AN3841.

 

Regards,

Mac

 

0 件の賞賛
返信

1,588件の閲覧回数
Bobli
Contributor I

Mac,

 

I have found the notes. Thanks very much for mentioning.

 

Bob

0 件の賞賛
返信