MCU bootloader dropped

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

MCU bootloader dropped

3,228 Views
jack_huang1
Contributor IV

Dear:

       Using NXP S9S08DZ60F2MLH to design a BCM, the project has been mass produced. Product software using Bootloader+ applications. All functions of the product are normal when it leaves the factory, but all functions of the product are invalid after the customer uses it. After receiving the faulty prototype, perform the following tests: 1. The bootloader connection program fails to connect to the device; 2. 2. The running indicator light of the single chip is off; 3. The test crystal has no waveform output, and the test phenomenon is the same after replacement; 4. After the bootloader is rewritten, the connection is normal. After the application is upgraded, the product functions are restored. May I ask the possible cause of this problem? Thank you.

 

0 Kudos
Reply
3 Replies

3,196 Views
vicentegomez
NXP TechSupport
NXP TechSupport

Probably your code was corrupted maybe by EMI/ESD.

 

Maybe the device was turned off when it was writing to the flash this can cause damage.

I recommend that you try to reproduce the problem in your facility. With this, you can decide the improvement that you can implement on your design.

 

There are some application notes about EMI and ESD on the nxp web page that can be helpful 

Regards

Vicente

 

 

 

 

0 Kudos
Reply

3,148 Views
vicentegomez
NXP TechSupport
NXP TechSupport

Ok, I will check it, but also I will delete it, because this is on the public community

 

0 Kudos
Reply

3,132 Views
vicentegomez
NXP TechSupport
NXP TechSupport

 I check the part of the schematics and it looks ok

Please let me know if you have more information

 

have a good day.

 

0 Kudos
Reply