MC9s08JM32 clock initialisation

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

MC9s08JM32 clock initialisation

2,272 Views
stevec
Contributor III

I have just decided to use the JM32 device because of its 24MHz max bus speed and 12 bit A/D, having used the 9S08RE16 device before. I am having problems understanding how to achieve this maximum bus speed. When I was selecting the device I thought it was just a simple job of running off a 48MHz crystal! Can someone point me in the right direction here. I wish to use an external crystal and have all internal processes working off 24MHz. I have tried using Device Initialiser within Codewarrior but to no avail.

 

Steve 

Labels (1)
0 Kudos
Reply
2 Replies

1,486 Views
pgo
Senior Contributor V

Dear stevec,

 

See this thread for some example code:

 

http://forums.freescale.com/freescale/board/message?board.id=8BITCOMM&message.id=13898#M13898

 

bye

 

0 Kudos
Reply

1,486 Views
stevec
Contributor III

Hi pgo,

 

Thanks for the link. Looks like it's what I need.

I'm a bit concerned about the reference to BDM speed. Something else I shall have to check out! I'm using a P&E MultiLink Interface. I've just found it works with a bus speed of up to 35MHz so I should be ok.

 

Steve

0 Kudos
Reply