MC9SO8 How to save RTC time bevor POR event occurse

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

MC9SO8 How to save RTC time bevor POR event occurse

2,084件の閲覧回数
joachimsasse
Contributor I

is there a method to save current time and date before a POR like reset pin, reset date and time to initial values?

タグ(2)
0 件の賞賛
返信
2 返答(返信)

1,708件の閲覧回数
joachimsasse
Contributor I

I use RESET Pin and PE. I watched that after RESET the initialization sequence copy the start time, hard coded from PE, to the variables holding time and the current time is lost. 

Is there a methode to save and copy the current time over PE sequence? 

 

0 件の賞賛
返信

1,708件の閲覧回数
tonyp
Senior Contributor II

Reset pin and power-on reset are two different cases. Which one do you really mean?

Power-on reset without some battery backup is not really possible. Unless you don't care for the date time staying frozen at the time of power down.


Reset pin: Just make sure you don't clear the variables holding the date time during initialization. Possibly add some CRC to verify correctness. Again, the date time will not remain too accurate over repeated resets out very long reset durations.

0 件の賞賛
返信