MC9S08PA4VWJ

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

MC9S08PA4VWJ

1,178件の閲覧回数
meghana_intern
Contributor I

how to write pwm logic for MC9S08PA4 microcontroller.i want to control led driver dim pin intensity using this microcontroller..if any sample code is available for this

ラベル(1)
0 件の賞賛
返信
1 返信

1,088件の閲覧回数
vicentegomez
NXP TechSupport
NXP TechSupport

You can use the following code to set the FTM2 (I use the pt60 )

FTM2_MOD = 8000; // PWM frequency is about 1 KHz8000

// Configure channel 0 to PWM mode (center aligned high-true pulses)
FTM2_C0SC = FTM2_C0SC_ELSB_MASK | FTM2_C0SC_MSB_MASK;
FTM2_C0V = 4000; // channel 0 set to 50%

// FTM clock = BUSCLK = 8MHz, Overflow Interrupt Enabled,
FTM2_SC = FTM2_SC_CLKS0_MASK | FTM2_SC_TOIE_MASK;

interrupt VectorNumber_Vftm2ovf void FTM2ovfISR (void)
{
//Clear interrupt flag

(void)FTM2_SC;
FTM2_SC_TOF = 0;
counts--;
if (!counts)
{
if (!up_down) //up counting
{
FTM2_C0V += 80;
if (FTM2_C0V == 3920)
{
up_down = 1;
}
//when reaching 99%, change to down counting
}
else
{
FTM2_C0V -= 80;
if (FTM2_C0V == 80)
{
up_down = 0;
}
//when reaching 1%, change to up counting
}
counts = OVF_COUNTS;
}


PORT_PTGD_PTGD1 ^= 1;

}

I hope this will help you.

regards

Vicente Gomez

0 件の賞賛
返信