MC9S08MP16 problem with upload program on it using BDM

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

MC9S08MP16 problem with upload program on it using BDM

2,101件の閲覧回数
pawelniewiadoms
Contributor I

Hello, I have MC9S08MP board and I have problem to upload program on it via BDM. I'm using CodeWarrior 10.6 and when I'm trying debug example program this window appears:118699_118699.pngpastedImage_0.png

When I reconnect it nothing happens. After click OK this appears:

118700_118700.pngpastedImage_1.png

Then it's just error when I click 'Abort'. OSBDM is visible in device manager and all drivers are installed properly.
Please help me with this problem.
Greetings,
Pawel Niewiadomski

ラベル(1)
0 件の賞賛
返信
2 返答(返信)

2,011件の閲覧回数
pawelniewiadoms
Contributor I

Problem solved, It was problem with one of resistors in my board which has short circuit. Thanks for responding!

0 件の賞賛
返信

2,011件の閲覧回数
Leojunin
Contributor IV

Hi Pawel,

check the bypass capacitor, there may be a lot of capacity in the power line and prevents micro finalize the POR. It would be nice some 100nF I have not tried more, but if I had that fails. You can skip this failure by setting the Power Down Delay longer. Example: 1S

Best regards

0 件の賞賛
返信