MC9S08GB60 Internal Number

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

MC9S08GB60 Internal Number

4,235 次查看
billp
Contributor I
Is there an internal unique number that is recorded in the MC9S08GB60 that I can read using C that would be unique with each CPU?
标签 (1)
0 项奖励
回复
3 回复数

1,602 次查看
mke_et
Contributor IV
If you have need of a peripheral, see if you can get a unique number from that.

I have a small weather device that I used a DS18S20 temerature sensor part on, and it's 1-wire address is perfect for providing a serial number on the fly for the entire unit. Hey, if you gotta have the part anyway, choose it wisely!

The only caveat is if you change that part... I've had 2 units where I had to change that part. One shorted out and the other was physically broken off the unit. (It sticks out to have the best response time to temperature changes.) I had to make allowances in my tracking software to be able to change that number 'on the fly' for repairs.

Mike
0 项奖励
回复

1,602 次查看
Alban
Senior Contributor II
No,
There is no serial number you can read.
However, some programmer are able to create one when the software is put into Flash in the programming house.
Cheers,
Alban.
0 项奖励
回复

1,602 次查看
bigmac
Specialist III

Hello,

P&E have a "Serialize" utility available from their web site.  This might do what you you require.

Regards,
Mac

 

0 项奖励
回复