MC9S08AW32 Clock Generator with 16MHz Osc

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

MC9S08AW32 Clock Generator with 16MHz Osc

3,444件の閲覧回数
jerryn
Contributor I

I am trying to use a 16 Mhz external oscillator for both the CPU clk and the BUSCLK, but am having difficulty in getting it to operate correctly.  The reason for wanting to use the external oscillator is so that no trimming of the internal clock would be required.

 

Using the internal clock, some chips exhibit baud rate errors without trimming.  I tried to use the initializer, to use the FBE mode, but the debug module fails displaying "frequency change to ~0 hz, repeatedly.

 

The setting from the initializer that works is

ICGC1 = 0x46

ICGC2 = 0x00

 

The setting that I tried to change to is

ICGC1 = 0x52

ICGC2 = OX03

 

Any suggestions?

 

Thanks,

Jerry

ラベル(1)
0 件の賞賛
返信
4 返答(返信)

2,157件の閲覧回数
bigmac
Specialist III

Hello Jerry,

 

Are you attempting to use an external packaged oscillator (single EXTAL connection), or an external crystal resonator (with two connections)?  If using the latter, the ICG1 setting is incorrect.  The REFS bit, and possibly the HGO bit, would need to be set.

 

Note that some of the bits of ICG1 are write-once only after a reset.

 

Regards,

Mac

 

0 件の賞賛
返信

2,157件の閲覧回数
jerryn
Contributor I

I am using a packaged oscillator.

 

I also noticed that after I program the chip and inspect location 0xFFBE, it already has a value in the range of 0x85-0x8A.  Where does this value come from?  I inspected the various startup code and MCUinit, and don't see where this value originates.

 

Jerry

0 件の賞賛
返信

2,157件の閲覧回数
bigmac
Specialist III

Hello Jerry,

 

The flash location 0xFFBE is designated as storage for the ICG calibration value, and this value should usually be loaded into the ICGTRM register by program code, to obtain a calibrated internal clock frequency.

 

It is possible that the calibration takes place automatically, during the flash programming process. The median calibration value is 0x80.

 

With respect to the previous problem, are there similar issues when you attempt to initiate and use FEI mode? I wonder if there are COP timeout problems, but this should occur for either ICG mode. Have you been able to verify that the packaged oscillator is actually producing output with the correct voltage swing?

 

Regards.

Mac

 

Message Edited by bigmac on 2009-04-08 05:11 PM
0 件の賞賛
返信

2,157件の閲覧回数
jerryn
Contributor I

Hi Bigmac,

 

Thanks for your suggestions.  I have a combination that works

ICGC1 = 0x54

ICGC2 = 0x01

The difficulty may have been with the Device Initiializer and the various sequence and changes that I went through before landing on this configuration.  I continually would get different warnings with various combinations of "Source CPU clock" and "External Clock"....it wasn't as straight forward as I thought it should be, although, again, it could have been a settings sequence issue.

1) Source CPU clock           External Clock 16.0 MHz

2) Initialize trim value         no

3) External Clock               Enabled

3a) Oscillator Frequency     16.0 MHz

3b) External Clock Source   External oscillator

4) Clock divider                 Auto Select

4a) Internal bus clock        4.0 MHz

5) FLL clock                     Disabled

 

The difficulty with the BDM mode "went away...???", and that could be due to getting the chip into some wierd mode.  The error message from the debugger was a repeated "changing frequency to 0Hz"

 

The "automatic" creation of the value stored for ICGTRM @ 0xFFBE looks like comes from the programmer, "CPROGHCS08 Programmer" , but since I am not using the internal clock, I think the point is moot.

 

Anyway, thanks for replying....it is nice to know that there is some help out there and people like you are willing to spend some time.

 

 

0 件の賞賛
返信