MC9S08AC32 Baking temperature, Soldering information

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

MC9S08AC32 Baking temperature, Soldering information

1,948件の閲覧回数
caesar_song
Contributor III

Hi Would you kindly help to provide the MC9S08AC32 Baking temperature, Soldering information,thanks

0 件の賞賛
返信
1 返信

1,936件の閲覧回数
vicentegomez
NXP TechSupport
NXP TechSupport

if you check the following link you can find all the package options for the S08AC devices,

https://www.nxp.com/products/processors-and-microcontrollers/additional-mpu-mcus-architectures/8-bit...

all of them are lead free I will take just as an example the MC9S08AC8MFGE that is a LQFP 44

on this link you will see that the peak of temperature is 260 C and this device is MLS 3

https://www.nxp.com/part/MC9S08AC8MFGE#/

so for the soldering we have the followin application note

https://www.nxp.com/docs/en/application-note/AN3300.pdf

 

Regarding to baking you need to follow the 

IPC/JEDEC J-STD-033 Bake Conditions

and depending the package that you are using is the time and the temperature that you need to use

 

0 件の賞賛
返信