MC68705R3 erase

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

MC68705R3 erase

1,732 Views
kamilica
Contributor I
Hi I am looking for solution to erase MC68705R3 chip. I have some with window on and they are UV erasable, but majority of them are without.
Labels (1)
0 Kudos
Reply
1 Reply

1,088 Views
peg
Senior Contributor IV

Hello and welcome to the fora, kamilica.

Presumably the windowed ones are also ceramic with a quartz glass window. This is expensive to manufacture (buy) especially when most devices will only ever be programmed once. Because of this they come up with "OTP" One Time Programmable devices which are the same inside but just molded in plastic. If you need to re-programme these, you throw it away and use a new one.

This is probably what you have. If you don't want what is programmed into them now they are worthless.

 

0 Kudos
Reply