MC34674 soldering help

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

MC34674 soldering help

2,324件の閲覧回数
mimco
Contributor I

Hi,

 

I know that this theme is not about MCU, but I don't know to which group belongs. I need hand-solder Lion charger MC34674, but I don't know how. I try solder 3 pieces but unsuccesfully. When I complete 2 PCB with this IC, after supply voltage and battery connection, the one LED was turned on, VBAT was 3.78V (after battery disconnect was this voltage around 2.5V), but Vref was still 0V and I don't know if this was caused unsuccesfull soldering or other error. Please any idea how proprely solder this IC?

 

Thanks

 

PS: I'm sorry for my poor english.

ラベル(1)
0 件の賞賛
返信
2 返答(返信)

1,476件の閲覧回数
MrBean
Contributor I

Looks like a DFN8 with exposed-die-pad. (pad in the middle of the package))

Die pad is used to cool the device, and MUST be connected to ground.

Have you soldered the die pad ?

Message Edited by MrBean on 2009-03-13 13:18 01:18 PM
0 件の賞賛
返信

1,476件の閲覧回数
mimco
Contributor I

Hi MrBean,
thank you for your answer. Yes the package looks the same like the DFN8 one. I've tried to solder EPAD to the ground but I don't know if I've succeded. I'm not sure how to test if it's done right. I've used different circuit instead after few failed attempts but I would like to try it again sometimes. Thanks

 

Best regards mimco

0 件の賞賛
返信