MC13213 schematic or gerber file

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

MC13213 schematic or gerber file

4,265 Views
Mercurio
Contributor I
Hi evreyone, i need to find some guide line about MC13213. I need to build a ZigBee device with a bipolar antenna and i need some exemple of schematic or gerber file to know which components i need and how to make right connections.

Can anyone help me?

Thank's to all.
Ciao
Labels (1)
0 Kudos
Reply
4 Replies

2,026 Views
J2MEJediMaster
Specialist I
Enter your part number in the "Enter Keyword" search entry at the top right of this page, and it will call up a bunch of entries for the MC13213. Scroll down until you find "1321xNCB Reference Design for the 1321x-NCB Dev Board". This archive file has a schematic and gerber files for a reference board using the part. This might not be exactly what you want, but perhaps it will get you started.

Good luck!

---Tom
0 Kudos
Reply

2,026 Views
Mercurio
Contributor I
Thank you very much, i've got yet something like that. What i need is an example using bipole antenna, but i can't find nothig with bipole.

Anyway thank you so much :smileywink:
0 Kudos
Reply

2,026 Views
Ware
Contributor III
 
The 13192-SARD board used a bipole antenna.  It used the MC13192, but the interface to the antenna should be the same as the MC13213.
 
Regards,
 - Ware
 
Message Edited by t.dowe on 2009-09-22 11:27 AM
0 Kudos
Reply

2,026 Views
Mercurio
Contributor I
Thank you so much :smileywink:

Ciao
0 Kudos
Reply