MC13213-SRB and acquisition...

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

MC13213-SRB and acquisition...

1,700件の閲覧回数
Ikoria
Contributor I
Hi all.
I'm Iko, from France (sorry for my english ^^)
 
I try to have information from various phone service but i don't find something...
 
I think i'll buy this dev kit (13213-SRN) for my application.
I try to send sensor value with zigbee. My sensor is a Force Sensitive Resistor (FSR: made by INTERLINK), it's like a various resistor.
 
In the comercial document, it's say "...The boards can also bypass the acceleration sensor to develop customized applications."
 
Then i have two questions.
 
First. Can i use this device to develop a card for acquire and send my sensor value? (the 10bit adc is correct for me) 
 
Second: Has i saw in various discuss, Transmittion rate is like "one data pack" by 1ms ?
 
Thancks for all your informations.
Beast regards.
Iko.
ラベル(1)
0 件の賞賛
返信
1 返信

1,181件の閲覧回数
Ikoria
Contributor I
Hello.
Sorry for the second post.

I have informations....

I can uses the development board 1321X-SRB .
There are analogue input with 3.3V max....

This is not writte anywhere...


See ya....
0 件の賞賛
返信