MC13193 documents

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

MC13193 documents

2,516 Views
wolverine
Contributor I
HI, I am a student in Cape Town and im using an MC13193 Evaluation kit for a project are the document of this kit any ware available?
Labels (1)
0 Kudos
Reply
2 Replies

1,568 Views
wolverine
Contributor I
Thanks Mark.

wolverine
0 Kudos
Reply

1,568 Views
UK_CF_FAE
NXP Employee
NXP Employee
HI Wolverine,
 
Obviously the answer to your question is yes.
The documentation for the MC13193 Evaluation Kit is available on the CD that came with the kit.
 
If this has been lost, you'll have some work to do.
 
I googled the 3 words MC13193 Evaluation Kit and got this:
 
 
Note that this is one long URL
 
EVK is made up of 2 main boards:
3-off SARD
2-off EVB
 
You'll find the documentation for those boards on the Freescale site.
 
Download the BeeKit, which contains all of the software for these boards, and the download contains plenty of information. Note that the SARD and EVB boards are deprecated now, and are not available as shortcuts in the BeeKit wizard. You'll need to use the platform editor to get support for the EVB and SARD.
 
Good luck.
 
Mark
0 Kudos
Reply