MC 13192 transceiver hanging while receiving and transmitting simultaneously

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

MC 13192 transceiver hanging while receiving and transmitting simultaneously

1,851件の閲覧回数
nightbird_iimc
Contributor I

Hi,

My objective is to create a cluster tree network where the end devices send periodic (say 3 seconds) beacons and the routers will forward it to the PAN Coordinator or to a designated router. All communication is done unicast.

I am facing a serious problem with the coordinator/Router (a FFD) receive and then transmit mcps packets on a periodic interval (say, while 3 devices are in range). the device (the mcu and/or the transceiver) is getting hanged after a while (irregular interval ranging from 2-3 minutes to 20 minutes). and calling the function PWRLib_Reset() doesn’t even work.

Let me explain my experimental setup in a bit more detail.

I am using MC 13192 transceiver, with HC08S MCU, along with the BeeKit(version 1.1.1.0) generated demo 6 application on the 802.15.4 codebase (BeeKit Mac Codebase ver 1.0.0) and customizing it.

The PAN Coordinator: It is kept as it is. All capability info field is set to 1.

The Coordinator/Router: I am starting it as just another PAN coordinator -

A.    pMsg->msgType = gMlmeStartReq_c;
        pStartReq = &pMsg->msgData.startReq;
        pStartReq->panCoordinator = TRUE;

B.    gCapInfoAltPanCoord_c = 0

The End Device: Have set  gCapInfoAltPanCoord_c = 0

The communication is happening but after a while (not regular) the routers are getting hanged.

I have tried setting the gMPibRole_c to 0x00, 0x01, 0x02 for end device, router, PAN Coord respectively. e.g.
    uint8_t value = 0x01
    pMsg->msgType = gMlmeSetReq_c;
    pMsg->msgData.setReq.pibAttribute = gMPibRole_c;
    pMsg->msgData.setReq.pibAttributeValue = &value;
    ret = MSG_Send(NWK_MLME, pMsg);

This did not show any difference.

                  I have also tried changing the gMPibPanIdConflictDetection_c attribute to FALSE. Also set the gMacEventPanIdConflict_c to 0 in the NwkMacInterface.h file, so that the PAN coordinator conflict wont occur (just in case) between the Router and the PAN coordinator and the end devices.

This did not solve the problem also.

Is the MC 13192 transceiver hanging a known errata while receiving and transmitting. I understand that the transceiver interfaces with the MCU with 4 SPI and it is in the streaming mode not packet mode.

The same hanging problem exists in the broadcast mode also.

I am desperately seeking some help to resolve this transceiver hanging issue.

If you require more information please let me know.

please help.
thanks,
Srideep.
ラベル(1)
0 件の賞賛
返信
1 返信

878件の閲覧回数
Mads
Contributor V
Nightbird_iimc:
 
you are using a quite old version of the the MAC and Beekit.
Please go download the latest software on www.freescale.com/zigbee
 
the latest version is Beekit 1.7.0.0 with MAC codebase 1.0.3.
 
It comes with a Beacon mode example code you should use as your starting point.
 
Br,
mads
0 件の賞賛
返信