MAC ADDRESS PRODUCTION PHASE

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

MAC ADDRESS PRODUCTION PHASE

4,587 Views
ITZI
Contributor I
Hello,
 
I use the HCS08GT60 micrcontroller. I would like to know which is the best tool to write down the MAC ADRESS in a production phase.
I think Embedded Bootloader is an efficient tool to write the MAC Address manually, but in a production phase maybe there is a tool to do it easily due to MAC Addresses are continuos (MAC Address1= MAC Address0+1). 
Thanks.
 
Labels (1)
0 Kudos
Reply
5 Replies

2,707 Views
ITZI
Contributor I
Thanks David!
 
I would like to explain better what I try to do.
I have built a ZigBee module with HCS08GT60(44pin) and the MC13193.
I have programmed it with the Codewarrior 3.1 IDE by the BDM multilink , but the MAC address is randomly generated (as I though).
I woul like to make this module a product, and so I buy MAC addresses,.
I would like to know which tools I need to write in each module its unique MAC address by a serialized way.
 
Best Regards,
Itzi
 
0 Kudos
Reply

2,708 Views
Alban
Senior Contributor II
Hi Itzi,
 
With the MAC group you'll get you can use the solution advised by Peg without any worry !
It can increment each time the MAC address to store int he device, like a serial number.
 
Cheers,
Alban.
0 Kudos
Reply

2,708 Views
ITZI
Contributor I
Thanks Alban!!!
 
I have some problems.
I  downloaded the prog08sz.exe (I think this is the suitable for the HCS08GT60 MCU, isn´t it?), but I am not be able to connect the program with the target.
Can I use the BDM HCS08/HCS12 multilink? If so, which class have I to select to connect the target?
 
Kind Regards,
 
Itziar 
0 Kudos
Reply

2,708 Views
bigmac
Specialist III
Hello Itziar,
 
My understanding is that the free down-loaded program prog08sz.exe from the P&E website can only program HC08 devices.  For HCS08, I believe you would need to purchase a different version from P&E.
 
Regards,
Mac
 
0 Kudos
Reply

2,708 Views
peg
Senior Contributor IV
Hi ITZI,
As the S08GT does not have any networking built in, I presume you are attaching something externally and then require to hard code a unique MAC address in to each units MCU flash.
Am I correct?
If this is the case and the MAC address is 16 bytes or less you could use P&E's Serialize utility.
Regards
David

Message Edited by Alban on 2006-10-29 02:16 PM

0 Kudos
Reply