M68DEMO908GB60E

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

M68DEMO908GB60E

3,637件の閲覧回数
Sher
Contributor I

I bought the 

M68DEMO908GB60E, which is MCU, MPU & DSP Development Tools DEMO BOARD MC9S08GB60.


However when I create a project in CODEWARRIOR it ask me to select


 

not sure which one to use, need some help.

 

Thanks in advance!

ラベル(1)
0 件の賞賛
返信
8 返答(返信)

3,445件の閲覧回数
peg
Senior Contributor IV

 

Hello and welcome to the fora, Sher.

 

Click the [+] next to HCS08G Family

Then choose MC9S08GB60 and you should be under way

 

The HC part of the part number (in front of the S) was dropped from the number some time ago, but is still often used in family names etc.

 

0 件の賞賛
返信

3,445件の閲覧回数
Sher
Contributor I

Peg - Thanks,

 

I followed you advise however I get the following screen as a result:

 

 

I only received an RS232 cable with this product, do I need to orderP&E hardware?

 

Thanks

 

0 件の賞賛
返信

3,445件の閲覧回数
peg
Senior Contributor IV

Hello again,

 

This old board, unlike many of the newer ones does not have a built in BDM adapter.

You will need an external one.

Whether you buy one from the likes of P&E or make one of the open source alternatives is up to you.

0 件の賞賛
返信

3,445件の閲覧回数
Sher
Contributor I

Hi Peg,

 

You mentioned about "making one of the open source alternatives",

 

Can you refer me to any links?

 

Thanks

 

0 件の賞賛
返信

3,445件の閲覧回数
peg
Senior Contributor IV

Yes!

 

Right here!

0 件の賞賛
返信

3,445件の閲覧回数
Sher
Contributor I

Hi Peg,

 

Thanks a lot for your reply.

 

I am very new to this subject, from your provided link,  which one I should choose, I checked a few did not see the schematic for building the hardware to connect my board vis USB or RS232 to my pc / Code Warrior::

 

 

Thanks

0 件の賞賛
返信

3,445件の閲覧回数
peg
Senior Contributor IV

Hello,

 

I am way out of touch with this stuff now. Best you post a question in that forum for further help with this.

 

0 件の賞賛
返信

3,445件の閲覧回数
rocco
Senior Contributor II
0 件の賞賛
返信