M&P Multilink

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

M&P Multilink

764 Views
Julian99
Contributor III

I have developed approximately 20 projects using S08 processors and CodeWarrior 11.1  with the P&E Multilink Universal FX debugger. I used an Intel-based MAC with Parallels VM running Windows 7. Everything worked Great!

I now have a new MAC , again running Parallels VM and Windows 11. (no choice). CodeWarrior loaded, but with a message about no device driver. It works fine, but the debugger is not recognised. On the old Mac, Windows Device Manager showed an entry "Jungo Connectivity/Windriver", but on the new MAC the device manager only showed an entry "MULTILINK". 

There are a number of suggested fixes but the proposed files could not be found,

Can someone please offer me a working solution, even if it means using a different debug probe.

 

 

0 Kudos
Reply
5 Replies

689 Views
luis_maravilla
NXP Employee
NXP Employee

Hello,

I would recommend on using the OS windows 11 for using CodeWarrior v11.1 this is the supported option, not virtual machines; as we can't guarantee that the CodeWarrior Tool work with Virtual Machines

To download the v11.1, Please refer to CodeWarrior for MCUs (Eclipse IDE) v11.1

Best Regards, Luis

0 Kudos
Reply

654 Views
Julian99
Contributor III

Sorry about my other post. I replied to the wrong post (one that I should have closed as solved). You will notice that I have been using CW under a VM for "Many years" and although you can't guarantee it, I know that it works. all I need is the Windows device driver for the Multilink. I think it's somewhere on the P&E website, but I can't find it. So far I have CW running with no problems under windows 11, running in the Parallels VM, loaded in OSX Tahoe.

0 Kudos
Reply

643 Views
luis_maravilla
NXP Employee
NXP Employee

As an option you could ask them in their support forum if they have it 

PEmicro Support Home

Best Regards

0 Kudos
Reply

726 Views
db16122
Contributor IV

If you update from Windows 7 to Windows 11, all the related driver may need to reinstall

CodeWarrior® for MCUs (Eclipse IDE) could be a good choice to select

CodeWarrior® for MCUs (Eclipse IDE) - ColdFire®, 56800/E DSC, Qorivva® 56xx, RS08/S08, S12Z - 11.1

0 Kudos
Reply

694 Views
Julian99
Contributor III

I hate Windows and I am not updating from W7 to W11 - it is a new machine (Mac M4) and W7 is not compatible so I have no choice.I have been using CodeWarrior for about 25 years. My question was "which drivers do I need for W11 and where can I find them? 

Just as a point of interest and nothing to do with this topic, AUTODESK products will no longer run on old Intel-based Macs, so Windows 7 - R.I.P.

0 Kudos
Reply