LC60: TPM Input Capture Interrupt to wake up MCU in stop3 instead of KBI?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

LC60: TPM Input Capture Interrupt to wake up MCU in stop3 instead of KBI?

1,889件の閲覧回数
BasePointer
Contributor II
Hi,
 
Can I use Timer Input Capture Channel Interrupts to wake up MCU in stop3 mode, instead of KBI without consuming much power?
 
10x
BP.
ラベル(1)
0 件の賞賛
返信
1 返信

991件の閲覧回数
Ake
Contributor III
Hi,
 
In the MC9S08LC60 manual, rev 2, it says:
 
"Stop3 can be exited by asserting RESET, or by an interrupt from one of the following sources: the real-time interrupt (RTI), LVD, ADC, IRQ or the KBI."
 
The TPM is not included though, so it seems it won't work.
 
Regards,
Ake
0 件の賞賛
返信