Implementing Position Algorithms Using Accelerometers Document - DEMO9S08QG8

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Implementing Position Algorithms Using Accelerometers Document - DEMO9S08QG8

3,735 Views
jmlist
Contributor I
Hello. I had a question regarding the documentation on 'Implementing Positioning Algorithm Using Accelerometers' (http://www.freescale.com/files/sensors/doc/app_note/AN3397.pdf) document. The document on page 7 refers to full source code for the application. However, there are several include files in this source code that are referenced but not included in the document or I can't find (adc.h,buzzer.h, SCItx.h). Does anyone know where these are located or if they can be?

Thanks for your help.

Justin


Message Edited by NLFSJ on 2008-10-15 04:32 PM
Labels (1)
0 Kudos
Reply
3 Replies

1,947 Views
jmlist
Contributor I
anyone? :smileyhappy:
0 Kudos
Reply

1,947 Views
Gust
Contributor I
Hola jmlist

Te puedo contestar en español? Bueno, espero que si, jeje.... el tema es que esa nota de aplicación la dan como un ejemplo de lo que se puede hacer.... mira este post

Re: Locating header files for source code used in DEMO9S08QG8


0 Kudos
Reply

1,947 Views
bigmac
Specialist III
Hello,
 
Here is the link to which I think the previous post was referring -
 
Regards,
Mac
 
0 Kudos
Reply