I want to find a car-grade chip with arctan computing function

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

I want to find a car-grade chip with arctan computing function

1,503 Views
ixhsun
Contributor I

The input signals are sin and cos signals. I want to use arctan calculation to convert them into angle data. I need to find a chip with arctan operation function? And I need to know how long does the arctan operation take?

1、I would like to ask if you have a chip with a CORDIC module?

2、Is there a chip that can calculate the arctan function? If so, how long does it take to calculate the arctan function once?

0 Kudos
Reply
1 Reply

1,429 Views
vicentegomez
NXP TechSupport
NXP TechSupport

Do you want to use an 8 bit device for that?

please check the S08D family

But maybe 32 bit devices is a better option

Regards

Vicente

0 Kudos
Reply