How to use Watchdog in Beestack

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

How to use Watchdog in Beestack

1,849件の閲覧回数
JACKCHEN
Contributor I
Hi ,
 
I want to use watchdog in Wireless UART based on beestack.
But it is too quick to reset by the 2^18 cycles of the bus rate clock in beestack, is anyone had any experience of using watchdog in the beestack. 
Thanks.
ラベル(1)
0 件の賞賛
返信
1 返信

1,050件の閲覧回数
Denn
Contributor I
Hi Jack,
 
If COP watchdog is too fast, then you can have a SW watchdog wherein you determine the timeout period and after its successful completion, you insert illegal opcode which will initiate an "illegal opcode" reset.(WD timer is incremented everytime in the System clock ISR is executed say for every 1ms )
 
You can refer the thread which uses the above technique.
 
Regards,
Denn.
0 件の賞賛
返信