How to erase the original program  0f  mc9s08??

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

How to erase the original program  0f  mc9s08??

4,361 次查看
秀娟林
Contributor I

The following pictures are happened when burned the program

标签 (1)
标记 (2)
0 项奖励
回复
1 回复

4,189 次查看
david_diaz
NXP Employee
NXP Employee

Hello,

Please be aware that your device could be secured or the device clock is wrong.

The MC9S08 Series include circuitry to prevent unauthorized access to the contents of flash and RAM memory. When security is engaged, flash and RAM are considered secure resources. Direct-page registers, high-page registers, and the background debug controller are considered unsecured resources.

In order to unsecure your device, please refer to the Chapter 4.6.5.1, page 87, from the Reference Manual from the following link:

http://www.freescale.com/files/microcontrollers/doc/ref_manual/MC9S08QE128RM.pdf

At last, I strongly recommend you check the device clock. If the clock is wrong then communication is impossible.

Hope this information will be useful for you.

Have a great day.

Best Regards, :smileyhappy:

David Diaz.

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复