How to erase the original program  0f  mc9s08??

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

How to erase the original program  0f  mc9s08??

6,968 Views
秀娟林
Contributor I

The following pictures are happened when burned the program

Labels (1)
Tags (2)
0 Kudos
Reply
1 Reply

6,796 Views
david_diaz
NXP Employee
NXP Employee

Hello,

Please be aware that your device could be secured or the device clock is wrong.

The MC9S08 Series include circuitry to prevent unauthorized access to the contents of flash and RAM memory. When security is engaged, flash and RAM are considered secure resources. Direct-page registers, high-page registers, and the background debug controller are considered unsecured resources.

In order to unsecure your device, please refer to the Chapter 4.6.5.1, page 87, from the Reference Manual from the following link:

http://www.freescale.com/files/microcontrollers/doc/ref_manual/MC9S08QE128RM.pdf

At last, I strongly recommend you check the device clock. If the clock is wrong then communication is impossible.

Hope this information will be useful for you.

Have a great day.

Best Regards, :smileyhappy:

David Diaz.

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply