How can i use internal flash memory in JM60 for MSD?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

How can i use internal flash memory in JM60 for MSD?

3,006 Views
eduardo1
Contributor II

HELLO,

It's possible to implement a project in MC9S08JM60 to use as a MSD with internal flash memory? How can i do this?

Labels (1)
Tags (3)
0 Kudos
Reply
2 Replies

2,920 Views
tonyp
Senior Contributor II

Does MSD stand for Mass Storage Device?

If so, yes, in theory.  In practice, no.  With 60K to host you application and storage you can no longer call it 'Mass', can you?

Look at AN3927

0 Kudos
Reply

2,920 Views
eduardo1
Contributor II

Yes, my mistake haha. I need to push some text file like a usb stick, read into the memory and erase file. Thanks for share the AN, i will read about it.

0 Kudos
Reply