How can I reduce MCU consumption? (s08)

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

How can I reduce MCU consumption? (s08)

1,494 Views
mehdializadeh
Contributor II

I am using MC9S08DZ96 microcontroller. Normally, when the program is running, 30 milliamps of current is consumed. I know I have to put the MCU in sleep mode. For this, I wrote a function that sets the relevant registers.

 

void stop3(){
	setReg8(SOPT1, 0x20U);                
	setReg8(SOPT2, 0x00U);                
	setReg8(SPMSC1, 0x1CU);               
	setReg8(SPMSC2, 0x00U); 
}

 


And now, with the `asm(stop);` command, I will take the MCU to sleep mode. I want the current consumption to reach 10 milliamps by lowering the clock and disabling different parts of the microcontroller.
With this method I have done, the current consumption did not decrease. Can anyone help me?


0 Kudos
Reply
1 Reply

1,481 Views
mehdializadeh
Contributor II

This problem was solved. Instead of calling function `_EntryPoint` again, I wrote a function in file `main.c` and called this function before the command `asm(stop);` 

 

void stop3(){
setReg8(SOPT1, 0x20U);
setReg8(SOPT2, 0x00U);
setReg8(SPMSC1, 0x1CU);
setReg8(SPMSC2, 0x00U);
}

 



Then, In `main()` I called above function:

 

while(1){
    if (T_Timer >= 10000){
    stop3();
    asm(stop);
    }
}

 


With this, the normal consumption, which was 60 milliamps, was reduced to 40 milliamps. which, if we don't consider that the LEDs of the circuit are on, it will significantly reduce the consumption.

0 Kudos
Reply