HCS908LL16/36/64, Battery Capacity, Battery Life Calculation Tool.

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

HCS908LL16/36/64, Battery Capacity, Battery Life Calculation Tool.

1,160 次查看
Eng8492
Contributor I

Where is the authoritative source that gives an AA alkaline cell a capacity of approximately 2800mAh with a 1mA constant load? What did Freescale use for a cutoff voltage?  This is the value predicted by the Freescale battery life calculation tool. A competitor's tool gives AA capacity as 2850mA.

 

I have read the Energizer and Duracell technical manuals and they do not give battery life or capacity for a 1mA constant load.

The charts start at 10mA load.

标签 (1)
0 项奖励
回复
1 回复

868 次查看
bigmac
Specialist III

Hello,

 

For an AA alkaline cell, a load of 10mA would be considered a light load - it is with much heaver loads that the capacity would begin to reduce appreciably.  For a primary cell, such as an alkaline type, the unit to unit variation of capacity would probably be subject to a wide tolerance, so the difference between 2800 and 2850 mAh would be negligible.

 

For a 1mA constant current load, I suggest that you use the manufacturer's discharge period for a 10mA load, and simply multiply by 10.  The number of hours would then represent the mAh capacity to the particular discharge voltage that you require.

 

Regards,

Mac

 

0 项奖励
回复